How can I connect the ECU simulation to a real CAN bus?

0 votes, average: 0.00 out of 1 (0 votes, average: 0.00 out of 1)
You need to be a registered member to rate this.
Categories: CAN Configuration Online since: January 4, 2019

Sometimes you need a connection to a hardware CAN bus also from the simulation. Do the following steps:

  1. Open the PCAN Nets Configuration program.
  2. Drop the PCAN_Ligth_SIMx CAN bus down from the simulation to the hardware CAN bus.