How do I build an application project in PDT?

1 vote, average: 1.00 out of 1 (1 votes, average: 1.00 out of 1)
You need to be a registered member to rate this.
Categories: Common, PDTTags: Auto Code Builder, Build Code, PDT Online since: January 18, 2019

In the PDT the construction process can be started via the Ribbonbar Build -> Build :

It can, depending on the option:

  • Auto-Code for all ECUs and Service Files
  • only Auto-Code
  • Auto-Code for one ECU
  • or only the nur the Service Files

to be generated.

the created files are stored temporarily under C:\ProgramData\Hydac\PDT\Output\CodeBuilderOutput .